My contact person
Select location

Search for application examples

Improve technology and reduce costs

For years the igus® motto has been "plastics for longer life®". By this we mean the production of innovative plastic products which reduce maintenance work, achieve technical improvements, at the same time as reducing costs and increasing service life, everything delivered immediately from stock.

Our customers were able to improve the technology and reduce costs in more than 590 applications.
Some examples:

Longest travel in the world - no more downtimes

The longest travel with plastic energy chain  

The e-chain systems® today clearly contribute toward reliability, as system downtimes, for example through cable breaks, are reduced to zero.

Cables defy heat, sun, rain and snow

LED screen  

Previously used cables from a competitor had failed; since then the temperature-resistant chainflex® cables are used; the larger-than-life size LED screen in Dallas functions in any weather.

Rough environment, high speed

Special machine construction  

Even in particularly aggressive ambient conditions like in this high speed machining center, energy supply systems prove their reliability.

Costs saved, machine
availability increased

Beverages industry  

As iglidur® plain bearings have a long service life, and in addition need not be lubricated and costs only a fraction compared to conventional bearings, 90% of the costs could be saved.

More than Euro 10,000 saved each year

Fully automatic tire fitting lines  

The previously used bearings were blocked and the shafts used to break. The lubricant-free igubal® flange bearings used instead have been operating since May 2007 without failure. This saved Euro 2,440 in repair costs and Euro 8,400 in machine stoppages each year.

Trouble-free operation instead of shaft destruction

Concrete pipe cutter  

Due to the dirt accumulation in the ball bearings, the balls were blocked and the shafts were destroyed. The concrete cutting machine has now run for over three years entirely free of troubles despite the extremely heavy-duty operation.

Search

Are you looking for practically tested application examples in a certain industry?
Here you can browse through already implemented applications and filter them according to your specifications.

Industry sector:
Case of application:


High speed camera positioning

The rail & Tracking systems are used wherever fast camera movements are an important factor as, for example, at sport competitions, but also at many popular events such as concerts, stage shows, etc.

High speed camera positioning    

Spotlight adjustment

The drylin® N flat guide in a special design provides for the adjustment of spotlights.

Spotlight adjustment    

Camera system

The spherical igubal® coupling between motor and camera dolly permits speeds up to 3m/s in curves.

Camera system    

Lighting crossbeams

Stroke movements of 36m height of a lighting crossbeam at the Royal Opera, London.

Lighting crossbeams    

LED screen

Temperature-resistant chainflex® cables in an LED screen.

LED screen    

Screen lifter for large displays

Lifting heavy loads

Screen lifter for large displays    

Tangible sound in the home cinema

Very resilient

Tangible sound in the home cinema    

Moving Head

The plain bearing used has a low frictional resistance and is low maintenance and lubricant-free.

Moving Head    

Camera jib

igus® goes to Hollywood - polymer plain bearings in a camera jib

Camera jib    

TV studio

For this TV studio, a semi-circular cable-roller assembly has been developed.

TV studio    

Ice sculpture device

Every day, an ice sculpture for the glittering world of Las Vegas is created here fully automatically.

Ice sculpture device    

Dragon robot

A robot as an actor: Tradinno is one of the main actors in Germany's oldest folk play the "Further Drachenstich".

Dragon robot    

Video wall

This video wall was built for a Dutch television station.

Video wall    

4D seats

Maintenance-free igubal® pedestal bearings are used in theatre seats; they are noiseless and operate reliably even at high loads.

4D seats    

Camera tripod

This adjustable camera tripod is usually used for cameras that have their centre of gravity well beyond the bearing axis.

Camera tripod    

3D camera

With this 3D camera system „3D RIG“, the focus was on ease of movement and maintenance freedom.

3D camera    

Camera dolly 2

Another newly developed dolly for camera movement is the subject of this manus® contribution.

Camera dolly 2    

Camera dolly 1

This camera dolly is very quiet and easy to adjust. Thereby it allows many variations of movement.

Camera dolly 1    

3D camera

Instead of using expensive 3D cameras, two regular cameras can be mounted on this device so that together they can generate a three-dimensional image.

3D camera    

Video wall

This video wall is simple to install and customize.

Video wall    

Lifting system

The lifting system "Spiralift" is used in theatres and concert halls all over the world to raise and lower parts of the stage, for example.

Lifting system    

Spotlight installation

This impressive spotlight installation was used on the South American tour of the Mexican singer Alejandro Fernandez.

Spotlight installation    

Television studio

This construction is used in a TV studio to realize different stage designs within a very short time.

Television studio    

Large format camera

This large format camera works absolutely precisely.

Large format camera    

Media technology

In this application an automated camera slide control needed to be built.

Media technology    
Applications overview

I have the following project - following question - following request

No application example has been found here for your special case of application. Would you like to have further assistance?
Please let us know how we can help you!



Your data

Please always complete the fields marked *.

Company:*
First name:*
Last name:*
Phone:
Email:*
If you would like to request catalogs or samples then please complete your address here.
Form of address:
Street:
Postcode:
Town:
Country:
State:
Yes, I would like to receive information on current products and services of igus® by e-mail. I agree to the exclusive use of my data by igus® in the framework of advertising messages in accordance with the data protection regulations. I am aware that I can withdraw my consent prospectively at any time by means of the "Unsubscribe" link contained in every e-mail.
I agree to the data protection regulations and the processing of my data. You can revoke this authorisation at any time.
Send